This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5158: 15V In 48V?

Part Number: LM5158
Other Parts Discussed in Thread: , LM5157, LM5156, LM51561

Hi,

I'm looking to design a 15V in, 48V out boost circuit.

I've looked at the following parts:

LM5158

LM51581

LM5157

LM51571

LM5156

LM51561

I have a few questions:

* The LM51581 has the lowest Peak Current rating (1.63A), what would be the maximum output current I could get out of this design?

* If I do a design for the LM5158/1, can I substitute the LM5157/1 if needed?

* Any reason to go for the LM5156/1 over the 57 or 58?

* Low noise on the output is important, do you have any resources to help with reducing it?

Thanks,

G