Other Parts Discussed in Thread: TPS274160
Hello,
I am using the TPS272C45 as follows:
VS = 24V
Logic Vdd = 3.3V, inputs driven by a micro
In the Absolute Maximum Ratings, some of the upper limits are specified as VS:
Our use case is such that VS might switch off at its source (power supply) independent of the 3.3V supply. So VS=0V in this scenario, and the inputs at 3.3V would be greater than that. Is this really going to be a problem?
I am also using the TPS274160, but am not seeing the same requirement:
Could you also confirm whether or not this is a problem?
Thank you.