Hi,
In my design
Vin= 1.8V
Vbias=3.3V
Vout= 1.2V
Iout= 1.5A
My concern is If Vbias voltage goes for 2.7V then will it affect my output current ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In my design
Vin= 1.8V
Vbias=3.3V
Vout= 1.2V
Iout= 1.5A
My concern is If Vbias voltage goes for 2.7V then will it affect my output current ?
Hi Santhoshwaran,
If Vbias is dropped below 2.7V, then yes during that operational period, the device may enter dropout causing VOUT to sag, and subsequently IOUT to decrease.
However, once VBIAS is reasserted the VOUT will then begin to regulate normally again and the output side of the circuit will recover.
Is there a specific reason you are concerned about your VBIAS rail having a brownout condition that would force it to fall over 18% from it's target voltage?
Regards,
John