Other Parts Discussed in Thread: LMR23630
Hello TI experts,
my customer now tests LMR23630-Q1 because of the field issue.
They want to get simulation result to compare with the failure one.
I already did webench in TI site, but I only got a result with very short time.
could you check the simulation results based on the condition below?
part no : LMR23630AFQDDRQ1
Vin : 12V
Vout : 7V, 3A
also I want to know that I can see pulse output if I zoom the output voltage like the screenshot below.
Best regards,
Chase