Hello TI experts!
I am having a problem on my customer board with the UCD9090.
After the board came out of mounting, I connected to ucd9090 and did not see it on the bus, but I got an error that it is in ROM mode. (When i click "Yes" in the first picture no changes, no device can't found.)
Following the instructions, I tried to get it out of the ROM mod, but it was unsuccessful. Сhecksum does not match with documentation.
Checked circuits:
V33D - 3.29V;
V33A - 3.29V;
BPCap - 1.78V;
Reset - pulled up.
I am attaching screenshots of the errors.

What else can I do to fix it?
Regards,
Andrey