This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62086: Operation at low currents

Part Number: TPS62086

In a project we have, we need 3.3V as output and the minimum input voltage that we have is 3.35V (from a Li-Ion cell output) and during this state we set our device into a deep sleep mode, getting a 120uA current consumption. The datasheet and workbench describe an efficiency and power cycle graph, but it does not show the behavior of the regulator with currents/loads under the micro amps range.

So, we want to know the behavior of the regulator during this low power consumption scenario.

Thanks