Dear
I'm designing a battery charger with your BQ21061 IC and protection circuit with your BQ29707 to recharge a small capacity (about 30mAh) Li-Ion battery. Inside the datasheet of the battery I found that the battery must not be never recharge when the voltage is under 2V. If the device that I'm designing will not be use for a very long time probably will be happen that battery voltage goes below 2V. The protection circuit (BQ29707) open the discharge circuit when battery voltage reaches 2.8V but if the battery will not be recharge for a long time after that protection circuit open the discharge mosfet, could be happen that battery voltage continues to decrease and falls below 2V. Reading the datsheet of BQ21061 I seem to understand that the battery charger attemps to recharge with pre-charge phase also battery with voltage under 2V and therefore this conflicts with the specifications inside the battery datasheet. I would like to know if I well understand datasheet of BQ21061 and, if not, if BQ21061 has a minimum battery voltage under that it doesn't start the recharge process. Or, to avoid that BQ21061 attemps to recharge battery with voltage under 2V, do I need to measure battery voltage with our micro and disable the BQ21061 with the charger enable pin?
Thanks