Hello E2E Experts,
Good day
Why is there a specific statement regarding this in section 8.2.2.1.2 of the datasheet that the resistors should be 1K - 50K? Here is the exact line from the datasheet "These resistors should be chosen from values in the range of 1 kΩ to 50 kΩ".
If RFBT was say 182K what is the concern with this?
Thank you in advance for your support.
Regards,
CSC