This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5156: does not work for a boost converter in LTSpice XVII after

Part Number: LM5156


After removing a "}" from the LM5156 library for LTSpice from the unencrypted model available, the system is not working despite copying it from the Webench tool.

The design is for a boost converter from 24 V to 48 V with a minimum input voltage of 20 V and a switching frequency of 500 kHz