This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ21061: /INT pin routing out from WLCSP package avoiding via-in pad solution

Part Number: BQ21061

Dear,

I would like to know if we can routing out the /INT pin of BQ21061 connecting this pin to NC1 and NC2 pins avoiding via-in pad solution. From your application note "Slua996" I understand that it is possible to routing out the /LP pin using NC2 pin and therefore I need to know if it is also possible using NC1. From BQ21061 datasheet it seems not possible to connect NC1 pin to any other signal (whereas for NC2 pin it is possible to connect it to /LP pin as mentioned inside datasheet).

Thanks