Other Parts Discussed in Thread: TPS7A20
Hi Team,
Would like to ask if the following REGULATOR has a smaller package that can be recommended? (SOT89?)
TLV1117-33IDCYR 800MA 3.3V SOT-223 SMD
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kygo,
TLV1117 does not come in SOT-89, its smallest package option would be an SON 4mm x 4mm.
I could provide you another alternative LDO, but I would need some more information:
1. What is your input voltage?
2. What is your output current?
3. What are the important parameters? (PSRR, Iq, noise, etc.)
4. Do you need the package to have leads?
Regards,
Andres
Hi Andres
Thank you for the support !
Hi Kygo,
Given the specs provided I would recommend TPS7A2033PDBVR which comes in a SOT-23 package and has very low noise.
TLV1117-33IDCYR | TPS7A2033PDBVR | |
Generic Part Number | TLV1117 | TPS7A20 |
Iout(Max)(A) | 0.8 | 0.3 |
Vin(Max)(V) | 15 | 6 |
Vin(Min)(V) | 2.7 | 1.6 |
Fixed Voltage(V) | 3.3 | 3.3 |
PSRR @ 100 KHz(dB) |
28 | 60 |
Noise(uVrms) | 411 | 7 |
Accuracy(%) | 3.75 | 1.5 |
Dropout voltage (Vdo)(Typ)(mV) |
1200 | 110 |
Iq(Typ) (mA) |
1.7 | 0.0065 |
Output capacitor type | Non-Ceramic | Ceramic |
Thermal resistance θJA(°C/W) |
104.3 | 187.1 |
Package size: mm2 | 46 mm2: 7 x 6.5 (SOT-223|4) | 5 mm2: 1.6 x 2.9 (SOT-23|5) |
Regards,
Andres