Other Parts Discussed in Thread: TIDA-01168
Dear, Ti.
Hello.
I'd like to get help with LM5170-Q1 IC.
Currently, for the nFault function in LM5170-Q1 IC, we have a problem that the nFault signal does not occur as high.
As I checked in another post on this site, there is no capacitor between SW pin and Breaker FET in our circuit, and there is a capacitor behind FET.
Our circuit works fine when 10kohm is applied to the syncout pin, but if 10kohm is removed, it will not work.
I think the conditions for nFault signal to fall from LM5170-Q1 IC are as follows, is that right?
1. UVLO<2.5V
2. LM5170-Q1 IC VCC<8.5V
3. Large capacitor between swpin and Breaker FET
4. High side, Low side FET failure
I'd like to ask if the nFault signal could drop for another reason.
Thank you.