Hi support team,
It seems that current is leaking to the output when the output current is limited.
J5: Open, J4: 9-10 short (0.6A), VIN_SYS1=24V (adapter capacity 3A), electronic load (3A) on output
The leaking current is 2.2Ap at intervals of about 4 seconds, as shown in the attached waveform.
With J5 connection (MODE=GND), it will retry and operate intermittently.
Is there a workaround?
Regards,
Dice-K