I am using the LMZ21701 regulator for 5V input with 3.3V output. When 5V input voltage is applied the regulator output voltage starts off at 3.3V but after about 1-5minutes the voltage fluctuates around 2.4-2.5V then eventually down to 0.7V. I can see my power indicator LED flickering on and off. I am using the circuit recommended by the Power Designer, see attached schematic.
Any ideas why it wont hold 3.3V with only 1 LED pulling about 15mA?