This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62084: High side mos Rdson

Part Number: TLV62084

Hi team,

My customer wants to know the minimum value of Vin when Vout is 2.8V, thus they need to know the maximum value of High side MOS Rdson. In datasheet it only shows the typical value, which is 120mohm.

Best Regards,

Peter

  • Hello Peter,

    Thank you for reaching out.

    Just for the clarification:
    "My customer wants to know the minimum value of Vin when Vout is 2.8V"

    Does it mean the minimum Vin in which the device still below 100% duty cycle. If yes, it depends upon the output current as well.

    Generally, we don't share information which is not in the datasheet. and also, Rds ON value varies with the Tj. 

    I would like to know the customer. Can you please share the information, you can also share the information via emial : m-shaik@ti.com

    Thank you,

    Regards,

    Moheddin.

  • Hi Moheddin,

    Let's discuss via email.

    Best Regards,

    Peter