Other Parts Discussed in Thread: TPS7A63-Q1, , TPS7B69-Q1
Hi team,
Does TI have a similar device with L99VR01? The customer just wants to use 3 bits to control the output voltage. don't need more voltage levels.
Normal voltage( 5V,3.3 2.5V)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Does TI have a similar device with L99VR01? The customer just wants to use 3 bits to control the output voltage. don't need more voltage levels.
Normal voltage( 5V,3.3 2.5V)
Hi Jimmy,
McKyla will get back to you as soon as possible tomorrow, thanks for your patience.
Hey Jimmy,
The L99VR01 also appears to be a watchdog LDO. Unfortunately, we do not have any automotive, watchdog LDOs with the programable output, but I would recommend the TPS7A63-Q1 this is a similar LDO to the L99VR01 in functionality and has an adjustable version in order to generate the three rails described above.
If the watchdog functionality isn't of interest, I would recommend the TPS7B69-Q1 it is an automotive grade device as well with fix outputs at the specified voltages needed. Additionally, we do have one automotive qualified programable output part the TPS7A47-Q1, however I do think that this device will likely be overkill for the application described. The select pins also function differently, but page 12 of the TPS7A47-Q1 datasheet section 7.5.1 helps explain a little better.
Let me know if you have any further questions.
McKyla