This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24735EVM-710: Q1 is damaged on the development board

Part Number: BQ24735EVM-710


What could be the cause of the Q1 MOSFET failure, the Gate shorted to the Drain, on the development board? I am running the board from a 24V power supply.

  • Hi, Roman,

    Q1 limits the inrush current when the charger is first powered on. It will experience high current and high voltage drop at the same time. The FET Safe-Operation-Area should be checked. 

    I would suggest you monitoring the inrush current amplitude and make sure it is within the FET SOA. Increase C8, for example, from 0.1uF to 0.22uF will slow down the Q1 turn on and lower the inrush current. 

    Regards,

    Tiger