Other Parts Discussed in Thread: AM2634, TPS62913
Hi Team,
We used TPS65381A-Q1 + TPS62913 to power AM2634 and encountered some issues. VDD6+62913 to power 1.2V core and VDD3/5 to power MCU 3.3V. The input of 65381 is 12V DC Source.
The problem is very strange: when we use this 65381+62913 integrated power solution, the MCU always stop running software. Then we also checked the 1.2V and 3.3V voltage condition, it seemed normal. And VDD6 is also normal. So we didn't find the cause of the problem.
Then we change to other discrete power solution(other DC/DC and LDO to replace 65381) to power MCU. It seemed all the problem disappear.
So could you kindly give me some suggestions to find the cause of this problem? What aspects should I check, could you give a check list?
Thanks
BRs
Kian