Hello,
The duty cycle of LM5035CEVAL is relatively high under light load (about 35%), Please help analyze the cause, Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The duty cycle of LM5035CEVAL is relatively high under light load (about 35%), Please help analyze the cause, Thanks!
Hi and thanks for posting to E2E - What is the duty cycle you are expecting? Please provide waveforms, schematic or description of input voltage, output voltage, frequency, topology, transformer turns ratio? The more information you can provide, the better TI is able to support you. You should also consider using TI Power Stage Designer as a way to verify theoretical duty cycle for any power stage. Power Stage Designer allows top level sim for most popular power topologies.
Regards,
Steve M
Hello,
The customer uses TI's evaluation board, the model is LM5035CEVAL, which is not a product developed by the customer;
Problem description:
1. When there is no load, the MOS drive duty cycle of the bridge arm is large. When the 36V voltage is input, it is about 35%. How is this achieved?
2. The drive dead time of bridge arms Q11 and Q12 is about 100ns. How to avoid common conduction?
3. How can C3-C6 capacitance be obtained? Is there a calculation method for transformer output inductance?
Hi
Regards,
Steve M