Other Parts Discussed in Thread: BQ25790
Hello,
BQ25730's datasheet shows that for 65W charging, you would need about 7*10uF capacitors on VSYS line. My application would require much less power usage - about 15W at max. Is there a lower input/output capacitance I'm allowed to work with in order to reduce the amount of components, or should I still use the same guidelines as with 65W?
Also, am I correct in saying that BATFET only protects the battery from the charger, but does not help in case of problems with the load? Would it work if I add another MOSFET to the BATDRV_n pin so that I would have 2 mirrored P-channels that could completely disconnect the battery in case of overcurrent\undervoltage when using battery only?
Thanks,
Eyal