Other Parts Discussed in Thread: CSD25480F3
Do we have a device with the same package as RE1C001ZP,
And the specifications are similar as RE1C001ZO.
Would you give me some device recommendation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do we have a device with the same package as RE1C001ZP,
And the specifications are similar as RE1C001ZO.
Would you give me some device recommendation?
Hello Shawn,
Thanks for the inquiry. The RE1C001ZP is a -20V P-channel FET in SC-89 package. Unfortunately, TI does not make any FETs in this package. Our closest recommended part is the CSD25480F3 -20V PFET in F3 FemtoFET package which is not p2p or footprint compatible. The TI part is 0.47mm2, so >4x smaller, resistance is 159mOhm max vs comp 3Ohm so nearly 20x lower TI has much lower leakage specs, 10x lower Idss and 200x lower Igss and yet still has gate ESD protection. TI has resistance rated to 1.8Vgs not 1.2Vgs.
Best Regards,
John Wallace
TI FET Applications