This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25940-Q1: Design Risk of Connect Fan

Part Number: TPS25940-Q1
Other Parts Discussed in Thread: TPS25940

Hi Expert

My customer want to use TPS25940 for Fan protection.

input voltage range is 13.2V~10.8V 12 TYP 

output is 12V/1.6A 

because the Fan is inductor load. so could you please help to check whether need special design for inductor load?