Other Parts Discussed in Thread: UCC21750
Hello,
I have following queries for UCC21750-Q1,
1) What is the duration of peak current sink & source for UCC21750-Q1?
2) On page 9, for load capacitance (CL) of 180nF, frequency = 1KHz, sink-source current = 10A.
If switching frequency is 100KHz, CL = 13nF (CL = Q/ V, 196nC/15V = 13 nF), then what will be the gate current sink-source capacity?
3) If driver output pins are shorted indefinitely causing short circuit condition, then still UCC21750-Q1 will sustain? Any internal protection is there?
Regards,
Abhishek D.