Other Parts Discussed in Thread: BQ25703A
Hello TI,
I'm encountering an issue while conditioning the gas gauge for two 20Ah batteries connected in parallel (Total capacity of 40Ah, and energy of 512Wh).
The problem occurs when I have fully charged the battery (using a BQ25703a charger device). The SOH suddenly drops from 98% to 1% several hours after the charging is terminated. Full charge capacity and SOC also drop to zero.
What could be the root cause and how can I resolve this issue?
Kind regards,
Aaron