Hi team,
Here's an issue from the customer may need your help:
The register is configured to charge current limit 2.4A, but the actual charge current is only around 1.6 a and cannot be increased. By changing the current limit of the register to 1.2A, the actual test can be around 1.2A. However, the charge current set cannot be reached when the current limit set exceeds 1.6A.
While charging, the register status is as follows:
The register configuration is as follows:
REG00:70
REG01:06
REG02:3D
REG03:3A
REG04:26
REG05:18
REG06:5F
REG07:B9
REG08:00
REG0A:C3
Could you help check this case? Thanks.
Best Regards,
Cherry