This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65132: I2C ACK, no response after small ball test

Part Number: TPS65132
Other Parts Discussed in Thread: STRIKE

Hi team,

When my customer did a small ball test with the whole phone, then they found that the TPS65132 failed, showing no positive or negative bias output, read I2C ACK, no response.

Small ball test: ball weight 160g, strike height 16~25cm, the strike points are distributed in all positions on the fuselage and distributed equally. Begin the strike test when the video is playing with SD card (E.g. simulating a scenario where a key is stamped onto the whole machine)

Circuit diagram:

Fail probability: 1F/15 when testing, and then they changed the failed IC to another system, it still failed. (issue follows IC)

Test waveforms:

Could you help check the rationality of experiment with our TPS65132 and do you know the reason which may cause I2C ACK no response?

Thanks 

Best regards

Lillian