This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61022: use with 3.3uH inductor

Part Number: TPS61022


Hi,

I'm using this part and have a ton of Coilcraft XEL5030 3.3uH inductors to use up. The datasheet says the TPS61022 is designed for 0.3uH-2.9uH. I've tested the 3.3uH and it appears to be working great, but as a sanity check is there any reason not to roll with it?

The 3.3uH still has a high saturation of 8.4A (and ripple will be lower) and a DCR of ~22mOhm. Losses at the lower voltage end of the boost will be a bit higher but I can live with that.

The application uses a maximum of 2.5A at 5V but isn't current protected other than the fold-current inside the TPS61022. My worry is the inductor could saturate under this condition leading to FET damage and hence my double check with an expert.

Regards,

Andrew

  • Hi Andrew,

    0.3u~2.9uH is just the recommended value that we have tested, if you use 3.3uH and have tested it without any problem, I think it also will be fine, because 3.3uH is not very far from the recommended value.

    Regards,

    Nathan

  • It's more for the valley current, ILIM_SW, which I read as 10A max. XEL5030-3.3u has a 8.4A saturation point, so I foresee a potential for the lower FET inside the TPS61022 to be destroyed.

    I have no current limitation other than the TPS61022, and it's fed by super-capacitors which will sink the 10A no problem. The condition shouldn't ever occur, it would need a USB device to short, but...

  • Hi Andrew,

    From my understanding, are you worried about the potential 10A from super cap may damage the inductor?

    The 10A current will always be or it just lasts for a short time? If there is only a short time, I think it not a big problem for inductor.

    Regards,

    Nathan

  • No, the inductor won't be damaged.

    The super-caps can supply anything short-term, 100A will be possible, so the only line of defence is the TPS61022. The datasheet says the max valley current that it trips at is 10A. At 8.4A the XEL5030-3.3u is has a 30% indutance drop.

    I've dived into the XEL5030 datasheet and Coilcraft as usual have come through, at 10A it has 2uH inductance, well within the TPS61022 operating parameters. I now think it'll work ok during a short.

    It would be good to have this verified by a DC-DC expert as it could be an expensive mistake.

  • Hi Andrew,

    Yeah I think so,  it is not a big problem.

    Regards,

    Nathan