Other Parts Discussed in Thread: BQ78350
Hi,
We would like to config our BMS (Li -ion, 7S1P, 4900mAh@25.2V) to support voltage base shutdown:
- Shutdown Voltage set to 2700mV
- Shutdown Time set to 20s
- PF Shutdown Voltage - 1750mV
- PF Shutdown Time- 10s
- Charger Present Threshold- 2000mV
The CUV:
- Threshold- 2500mV
- Delay- 2s
- Recovery- 2750mV
Do you see any conflict between the battery base shutdown voltage level and the CUV Threshold?
BR