Can the POE Gigabit network transformer switch the corresponding signals of TD1 and TD4?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the POE Gigabit network transformer switch the corresponding signals of TD1 and TD4?
Hi Xiaofu,
Thanks for reaching out to us!
For me, from the circuit inside the transformer, there is no difference of TD1 and TD4 for data transmission as well as the data sending and receiving side are on the correct location. From the aspect of PoE in which the paired twisted wires are used, please make sure the PR12 - PR36, and PR45-PR78 are grouped.
Updated on Jan/17/2023: It has been a relatively long period that we have not received your reply. I will close this thread for now. Please open a new thread if you have further questions.
Best regards,
Diang