Other Parts Discussed in Thread: LM25148
Dear Sir,
Equation (22) shown in datasheet page 16, why there is a "220ns" item?
Best regards,
Genie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
toff_min is from drive circuit, in real application, it also have dead time between high side and low side drive and other delay , so considering these factor, adding 200ns will make enough margin
Thanks
Hi
I don't know the wenbench internal logic for frequency setup. but if your condition is12V input and 11V output, I more suggest you can take look at LM25148.
it support 98% duty cycle when Vin close to Vo.
Thanks
HI
yes, I think it more depend on your hardware result, you can put 147K in your porotype , if you see the output regulation is poor at Vin=12V, you can adjust the frequency lower, it won't impact other passive component if low down to 115Khz