Other Parts Discussed in Thread: TPS25750,
Hi
using the BQ25792 device without the TPS25750.
when i'm trying to charge after a few seconds the VBAT_OVP_STAT bit in register 20H and VSYS_OVP_STAT bit in register 21H are set to '1'.
in this state, the battery is being discharged.
nothing i'v done or wrote to the registers helped accept changing the VINDPM_7:0 value to higher value then should be.
at that state, there is no charge or discharge from the battery.
Thanks
Inon