Other Parts Discussed in Thread: BQ25720
Would be nice if we could use the bq25708 to power a 100 watt system.
The input voltage will be 12V or 20V, depending on the user implementation, and will have a 4sXp battery.
Is it as simple as reducing the sense resistors to something like 5 milliohms and using better FETs and a higher current/lower loss inductor? Obviously we will have to scale the register reads and writes to account for the change to the sense resistors.
Appreciate your help