This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: CC Reading of bq76940

Part Number: BQ76940

Hi,

The CC fresh data is updated every 250 ms, and triggering of  alert signal of CC Ready.

If the current is set to 2 Apm for instance, what data i will expect  when i read coulomb conuter in between two CC Ready signals severals times,  for example each 50 ms, reading the coulomb.

I mean the datas are available for reading in this time periods regardless of CC Ready? 

best regard