Other Parts Discussed in Thread: LP5860EVM
Hello,
My customer is looking at the LP5861 device and has some questions around power consumption at low output currents. Their concern:
One concern might be the current drain, the first page in the spec sheet says the average current is 3 mA typical for 5mA of channel current, but the electrical spec table lists 4.3 mA for 5mA of channel current. Is the difference how the device's 5mA output current is programmed? For example, maybe it is is higher when current is limited by the global max current (MC) instead of individual dot current (DC)?
Is there anything that can be done to to minimize Icc? Lastly, can we share any data on Icc for low (sub 1mA) channel currents? I don't see anything showing how this might vary with channel current in the datasheet. Customer plan is to run all the LEDs at around 0.5 mA, and they are hoping the IC current might go down with lower output currents.
Thanks!
John