Other Parts Discussed in Thread: PCF8575
Hello
I have a custom board on which the FLT pin of the TPS26625 is directly connected to an IO-Expander PCF8575 input. There is no additional resistor in line or a pull-up or pull-down resistor. The PCF8575 is connected to 5.25V supply. The problem is that if there is no error reported (The fault pin doesn't pull to low.) The measured voltage is only 3.6V on the iSUP1_nFLT signal and not the expected 5.25V.
The PCF8575 has an pull-up current between 30..300uA. The leakage of the FLT pin according to the datasheet is around 100nA. So this shouldn't be a problem. Does anyone have an idea why the voltage is so low?
Best regards
Andreas