Hi team,
My customer wants to use LM25184 to design. Can LM25184 support below 2 condition power?
- LM25184 input :10~42VDC output:5V@ 2A
- LM25184 input :10~42VDC output:15VDC + 15VDC @0.5A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer wants to use LM25184 to design. Can LM25184 support below 2 condition power?
Hi Jimmy
LM25184
LM25184 can support the 5V@ 2A design. But for the 15V+15V dual output design, the output capacity is around 13W according to the fast calculation tool. Actually, the output capacity can be larger if the Vinmin is larger. You can find the calculation tool on ti.com.
LM(2)518x PSR flyback converter quickstart tool revA2.xlsx
Best regards.
Hi Jimmy
Yes LM25184 can support dual output with different ground.
Best regards.