This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55010: Withstand voltage level of TPS55010

Part Number: TPS55010

Hi,team,

My customer asked a question, please help answer it, thank you.

GB 9706.1 General Requirements for Basic Safety and Basic Performance of Medical Electrical Equipment

This standard requires that the input Vin shall be short circuited to the ground, and the low-voltage level of output vout or gnd shall be above 1KV. Previously, it was 500V, and the new standard was raised to 1000V.

My customer want to know whether the TPS55010 meets the above requirements? If this chip is not suitable, can you help to recommend chips that meet the requirements.

V in is actually 3V to 4.5V, output 3.3V, I out ≥ 200ma, boost/buck voltage rise/drop mode.

Best Regards,

Katherine