1.the maximal spec of ripple is 13mV
The actual messurement is 15.6mV (Vout: 1.2V & Vin:12V: Iout:26A) & 16mV (Vout: 0.85V & Vin:12V: Iout:18A) which does not meet the criteria 13mV
How to explain the overspec? like the difference of Oscilloscope or the influence of probe
How to improve the measured ripple?
Test Conditions:
(1.) Set Oscilloscope BW= 20MHz and AC coupling mode.
(2.) Measure at the pins of the dc-dc output MLCC capacitor .
(3.) The outputs will be bypassed with one 0.1uF and one 10uF MLCC (type X5R) capacitors.
2.the spec of In-rush current
3.the spec of Timing and power on
4.Over current protection:
The range is 35.7A~48.3A? Because of +/-15% of 42A (Overcurrent threshold)
5. Current de-raing cannot be measured ?
Because indcutor is embedded in power module and there is no spec of current de-raing
Test Conditions:
1. Critical components must have the right rating and are used safely.
2. It is performed at the maximum DC current margin at Maximum Load condition.
3. Set Oscilloscope BW=Full bandwidth.
4. If multiple max load conditions are defined the worst case condition must be considered.
Critical components must have the right rating and are used safely.