Other Parts Discussed in Thread: TPS61091, TPS60120
Tha tps60204 datasheet states it can deliver (min) 100mA continuously.
I want to power a esp32C3 microcontroller (in low power mode).
However, during bluetooth transmissions it will draw tiny peaks (say 2ms each 250ms) of max 180mA.
I have measured the device with a power profiler, and the peaks are tiny, minimum power draw is about 16mA, max 180mA and average is 25mA.
There are no big timespans where the power is above 100mA (even above 50mA).
Can I then use this device? Or should I switch to TPS61091 for example.
This seems a bit of an overkill for my application...
My device is battery powered 2x AAA alkaline.
I like to use the low-battery warning on the TPS60204.
Any other recommendations?
Thanks in advance