Hello
We are using UCC37324 to drive an array of parallel N-channel MOSFETs on the low side. The IC is supplied by 12V at VDD. Logic high at INA and INB is at 3.3V.
The distance between output terminals (OUTA and OUTB) and the first N-MOSFET in the array is about 45mm. Does this affect the IC operation?
Issues we are facing:
1. OUTA and OUTB show 12V when INA and INB are given logic high signals.
2. Voltages across INA and INB are fluctuating between 1.5V to 0V.
3. MCU operations are being halted.
Whent the IC is depopulated off the board, MCU operations are normal. Could the distance, as mentioned above, cause these problems?
Your help is highly appreciated.
Thanks & Regards