This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS613221AEVM: Backfeeding TPS613221ADBVT with parallel source

Part Number: TPS613221AEVM
Other Parts Discussed in Thread: TPS61322

I asked this about another converter, but I wanted to make sure it's okay for this one as well.

Is it okay to backfeed the OUT pin with a 5.0V parallel source, both when there is an input voltage on the SW pin and when it is disconnected?

Will the converter conduct current in reverse when I do this?

Thanks!

  • Hi Andrew,

    What is your 5 parallel source? Is it also a boost?

    TPS61322 doesn't have true disconnection, so it is like you connect a inductor and a diode parallel with the 5V source.

    So if the VIN < VOUT, diode will not conduct, I think this would be no problem.

    If the VOUT > target VOUT of TPS61322, also no problem.

    If the VOUT < target VOUT of TPS61322, device will switch and there may be some abnormal behavior. 

    Regards,

    Nathan

  • Great, thank you. The 5V source is USB. I hope to connect it without having to worry about disconnecting the battery (single cell NiMH) from the converter. Part of my concern was that if the battery voltage was very low it might be out of spec to have a parallel source on VOUT. VOUT will always be higher voltage than VIN, so it sounds like this will be fine. As you saw in my other question, I'm also considering other converters with an EN pin (like the TPS610994), but I assume the behavior is similar for all of these, i.e. they can all handle a parallel source on VOUT that is higher than VIN?

  • Hi Andrew,

    For TPS610994, if EN is high, the results will be as same as what I have said above. If EN is low, because of true disconnection this device has, there will be no path between VIN and VOUT, so it sill no problem regardless of VIN VOUT.

    Regards,

    Nathan