This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61256C: Power up under high current load

Part Number: TPS61256C

Hi. I am planning to use this part with a current load of 900mA at 3.3V. Will I experience the same power-up issue (related to load start-up current or pre-charge current limit) as the version of this part without the "C" at the end? The enable pin will be connected to the 3.3V input voltage. 

Thanks.

  • Hi Rafael,

    TPS61256C still have pre-charge current limit, so I am afraid that it may not support start-up with 900mA load.

    Could you please tell me about your VIN range? We can recommend some other devices with larger start-up current.

    And more, is you load a CR load or CC load?

    Regards,

    Nathan