Hi,
I am probably missing something obvious here:
I bought an LM5066EVK and am using the PI-Commander GUI (also tried the SPM_GUI, same result) to play around with it. The board is detected fine as LM5066EVK; I can set the limits, turn on and off, the measured Vin and Vout is also accurate, temp values seem plausible, all fine.
But the IIN value (and consequently, also the PIN value) is nonsense: IIN is not even close to what I measure with a multimeter; when the switch is turned off, it still measures around 150mA where it should be more like 7mA. If I turn the switch on, the IIN it measures is also way too high, but with a different offset (then it's more like 170mA too high, so it's obviously not a fixed offset that I can just substract).
I can read out the telemetry data via I2C and calculate the values as per the formula with the various coefficients in the data sheet and get the same results the GUI displays, basically.
Now, I could start fiddling around with the parameters, doing my own fit and so on to get the correct m, b, R and so on, but I don't understand why that should even be necessary. Shouldn't all the parameters be set up properly for the EVK already? In the GUI, it has all the correct values for Rs, Rdson etc., so everything matches the EVK BOM. So my thinking is the GUI should be set up correctly and it should in turn also set up the device correctly to work "out of the box". I also have no direct influence on the formula parameters the GUI uses except changing component values to something they obviously aren't.
The EVK is un-altered, meaning I did not change any of the components and all DIP switches are set to their defaults. I am switching a 48V source (which is what the EVK was designed for).
What am I missing here? Is this just an artifact of the +/- 4.5% measurement accuracy when I have a small load?
Greetings,
Sean