Other Parts Discussed in Thread: LM5642
Hi
Could you help to confirm whether LM2647 can replace LTC3865EUH#PBF, thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Whether the LM2647 can replace the LTC3865 will depend on the customer use case.
If customer needs greater than 28V, less the 5.5V or Sync pin then no.
The LM5642 may be a better device
|
|
LM2647 |
LTC3865 |
|
Input Voltage |
5.5V to 28V |
4.5 to 38V |
|
Output Voltage |
0.6V to (30% of 5.5V, 50% to 15V, 28% of 28V) |
0.6 to 5V |
|
# of Outputs |
2 |
2 |
|
Switching Frequency |
200kHz to 500kHz |
250 to 770kHz |
|
Mode |
FCCM and Skip |
FCCM, Burst or Skip |
|
Sync to ext clock |
N |
Y |
|
Supply Current |
1mA |
3mA |
|
Package |
TSSOP-28 9.7x6.4 28-WQFN 5x5 |
5x5 QFN |