This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5064: Resistance of Power Good pin (Pin 28)

Part Number: LM5064


Hello,

When turning on the board, GATE pin comes out and MOSFET V1175 is on.

UVLO shows high, OVLO is low, Voltage on MOSFET is 0.15V. PG has 10V pull-up with 5kohm. 

A Question is PG show low. 

What condition makes this is possible?

Please advise me.

Regards,

Moon