Other Parts Discussed in Thread: LM25149
I'm looking for a device with similar performance.
VIN = 24V±20%
VOUT = 12V±5%
IOUT = 2A (TYP, the MAX is still undefined)
However, we would really like to use an external FET to keep the DC/DC package temp low.
Any similar devices that can be used with an external FET?
Regards,
Darren