Hi,
We use LDO TPS74501PQWDRVRQ1 in our design, Vin=5.8V / Vout=3.3V. We caught an inrush current during start-up. The max is 632mA. Can you help to check if any side-effect? Will the current damage the LDO?
Regards,
Hsing
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We use LDO TPS74501PQWDRVRQ1 in our design, Vin=5.8V / Vout=3.3V. We caught an inrush current during start-up. The max is 632mA. Can you help to check if any side-effect? Will the current damage the LDO?
Regards,
Hsing
Hi Hsing,
What are your input and output capacitors?
The inrush seems somewhat odd as we would expect a shorter duration time for the inrush. The biggest concern is that it could trigger Current Limit if this duration increases.
It doesn't seem to be a big issue since Vout is not being pulled down. Have you verified that Vin rail doesn't see a drop? I recommend looking into the FAQ below as well as extra information:
Best,
Edgar Acosta
Hi Edgar,
Thank you for the reply. The capacitors are Cin=10UF /Cout=10UF+ 4.7UF*4pcs.
The current becomes small after the inrush current. So, If the current limit is triggered during start-up, Vout should be back to normal(3.3V) after the inrush current. That is what I thought. If it is correct, we can accept this situation.
Regards,
Hsing
Hi Hsing,
Yes, once the device recovers from current limit event (if any), then it should regulate as expected assuming there are no other issues.
In the case that inrush is still a concern here are some methods to reduce it:
Best,
Edgar Acosta