Other Parts Discussed in Thread: AM2434
One of the case, If using AM2434 (Sitara) ×2 and need full performance, 0.85V of VDD_CORE and VDDR_CORE need larger than 3A and LP87334D's BUCK0 have not enough to current rating (3A_max).
When above case, is one side BUCK0 substitute to common DC/DC converter no problem? (On the premise that sequence control is match)
Or, are both side BUCK0 substitute to common DC/DC converter OK, too? (LP87334D's BUCK0 is unused)
We referenced by below application note page 10, but these are one chip solution.
https://www.ti.com/jp/lit/an/slda059/slda059.pdf
Best regards,
Satoshi