Part Number: TPS23754EVM-383
Hi,
We meet the issue that EMC RE fail on 36MHz~42MHz (Over 3dB)

Attachment is PD part schematic refer to TPS23754EVM-383.
We had tried the ways :increase the value of R59 ; add RC snubber on U25....but there is still no inprovement.
Could you help to provide the other way?
Can U8 filt the frequency?
Thanks
Wendy