Hi, I designed a battery charging circuit using BQ25895MRTWR IC
when the battery is drained completely (0V), and if we give the power, the ic is not charging the battery it is reaching a voltage level of 2.99V (3V) and stops, without reaching a specified voltage I can only set the values in the i2c registers.
Details of the battery is as follows.
capacity:5000mAH
battery voltage:3.7V-4.2V
link: https://www.innovoya.com/product-page/955465-5000mah-rechargeable-lithium-polymer-battery-cells-1
I am also attaching the schematics for your reference.